Skip to Content


Content

Question 01

Can I mount the valve and actuator in an Explosion Proof (EX) environment?

Pneumatic actuators are inherently safe, so they can be mounted in EX environments. Our electronic actuators are not suitable for EX environments, and there are currently no plans to develop EX actuators for our valves or dampers.

 
 

Question 02

How do I select a valve for a steam system?

Flowrite 599 Series valves can be used on steam systems with an inlet pressure to 100 psig, with a maximum differential pressure of 50 psi.
The goal of steam system design is to condense all of the steam in the radiator or coil, and return only liquid condensate to the boiler. Doing so capitalizes on the high energy transfer associated with fluid change of state. The coil energy transfer rate is directly proportional to the mass flow rate of steam which enters the coil; hence a linear characteristic control valve is preferred. The trim material should be selected according to the pressure drop across the valve: <25 psi, brass/bronze; <50 psi, stainless steel. Choose the packing material according to the maximum inlet steam temperature: <250°F, EPDM O-ring; <337°F, Teflon V-ring.

Most of the H.V.A.C. steam systems will use saturated steam. Some systems will use superheated steam. Most systems will be two-pipe systems. Occasionally an old one-pipe system may be encountered - condensate return is difficult in these systems and may cause water hammer. On AHU coils, Siemens Building Technologies recommends 1/3, 2/3 control to improve control at low load, and extend life of valve trim by minimizing wire drawing. Use the steam valve sizing formulae for most accurate results. This formulae can be found in the Siemens HVAC Products catalog. Remember to use ABSOLUTE pressure, not gage pressure, in all steam sizing!

 
 

Question 03

How do I order a non-standard Flowrite 599 Series valve and actuator as a factory assembly?

The best solution is to order the valve and actuator separately and field assemble. For large quantities, call your Siemens sales representative for a special order.

 
 

Question 04

I have an old 591 series Powers valve with an 8" pneumatic actuator. Can I replace the actuator with a Flowrite 599 series actuator?

The 591 series is not compatible with the new Flowrite 599 series, however Siemens still does offer replacement actuators for the 591 series. All of the replecements parts can found in the Siemens HVAC Products catalog part number 144-001.

 
 

Question 05

Why did the face to face dimensions change on the 2 ½" to 6" Flowrite 599 series valves?

In 1996 Siemens Building Technologies, like other major valve manufactures made the change to conform to ANSI/ISA S75.03 face to face dimensions.

 
 

Question 06

Can Flowrite 599 valves be used for different flow media, such as air, diesel fuel, 40W motor oil, bromium hydroxide, or be made with a silicon free packing?

Yes, most non-corrosives can be handled with a special o-ring in the packing and/or a special gasket, and a silicon-free valve packing can be made. Contact your Siemens sales representative for a special quote.

 
 

Question 07

Are all the Flowrite 599 Series valve actuators interchangeable?

No, You must match the actuator stroke to the valve stroke if ordering the valve body and actuator separately. The Flowrite 599 series valve bodies from ½"- 3" have a ¾" stroke, 4" - 6" have a 1 ½" stroke.

 
 

Question 08

Can you install a Flowrite 599 series valve actuator outside?

The SKB/C weather shield is the first device, that when used in conjunction with the SKB or SKC Flowrite 599 series valve actuators, will give valve actuators a NEMA 3R degree of protection. The weather shield has been tested to protect these valve actuators against a variety of conditions -rain, sleet, ice and hail. It also offers protection against direct exposure to sunlight.