What kind of stall protection do these actuators have?
All motors in the OpenAir line have stall protection to improve reliability, to reduce power consumption, and prevent motor burn-out in the event a damper seizes.
In modulating damper actuators, 20 seconds after the torque limit has been reached, the motor switches off. Every 24 hours a new start begins checking to see if the condition still exists.
The 3-position floating, non-spring return damper actuators do not have a timer. Instead, they use a magnetic clutch to limit torque. These floating actuators are rated for 100% duty cycle.