Skip to Content


Content

For the business press

Siemens to Implement U.S. Army’s Largest Solar Photovoltaic System at White Sands Missile Range

Washington, Thursday, February 02, 2012

WHITE SANDS MISSILE RANGE

Solar Array Part of a $16.8 Million Energy Savings Performance Contract

Siemens Government Technologies, Inc. announced today that the U.S. Army Engineering and Support Center has awarded a $16.8 million task order to implement energy-conserving upgrades, including a 4.465 MW solar photovoltaic (PV) power generating system—the largest to date for the U.S. Army—at the White Sands Missile Range, N.M.

The solar PV system is the primary component of the energy savings performance contract (ESPC) to be implemented by the Building Technologies Division of Siemens Industry, Inc. The solar PV system will provide the Army with approximately 10,000 solar renewable energy credits annually as well as qualify it for a 30 percent federal cash grant in excess of $4.8 million. According to the U.S. Army Corps of Engineers, the solar PV system will help White Sands Missile Range achieve 10.8 percent renewable energy by the end of 2012, up from .5 percent and beating the 2013 government mandate by more than three percentage points. This project supports President Barack Obama’s directive that federal agencies use ESPCs to make $2 billion worth of energy efficiency upgrades over the next two years, as well as supporting the Army’s renewable energy goals.

 “This project implements a solar photovoltaic array system that will partially offset White Sands Missile Range’s energy requirements, improve facilities and operations, demonstrate Army engineering and technology capabilities and align with the Army’s Energy Security and NetZero objectives,” said Judy Marks, President and CEO of Siemens Government Technologies, Inc.

White Sands Missile Range is a Test and Evaluation Command Installation operated primarily for the support of research, development, test and evaluation of weapon and space systems, subsystems and components. Encompassing a missile range/rocket launch range, White Sands is one of the largest military installations in the U.S. covering 3,200 square miles. The facility is unique in the fact that it has several agencies on site as tenants including NASA and the U.S. Air Force.