Skip to Content


Content

For the business press

New Facility Prime IPad Application Ready for Prime Time Mobile Building System Transparency

Buffalo Grove, IL, Monday, January 23, 2012

Siemens Building Technologies Division announced today the launch of its Facility Prime™ native Apple iOS application for the APOGEE® Building Automation System (BAS). Through customized screens, Facility Prime enables fast, convenient, mobile interaction with a multitude of facility conditions.

Facility Prime goes beyond accessing data and provides two-way interaction between users and the building automation systems they manage. Siemens’ versatile application connects users to APOGEE BAS control and monitoring functions via wireless network connectivity. The application directly interacts with BACnet/IP and Siemens APOGEE P2 field panels.   

Users can develop their own customized interface graphics using Facility Prime Editor or, if desired, have their local Siemens representative create a dynamic interface to suit their facility management needs. After accessing the network, users can view environmental conditions via this custom-tailored interface.  Users can also connect to their facility’s BAS via the enterprise’s virtual private network if available. After proper access credentials are authenticated, users can command points and equipment.  Commands made from Facility Prime are logged in the APOGEE Insight System Activity Log.

Facility Prime delivers a variety of convenient, but powerful facility systems management features to the dynamic iPad platform including: 

Facility Prime becomes available in February. For more information contact your local Siemens Building Technologies representative or visit: