Eastern Kentucky University Energy Efficiency Project Grows To $27 Million After Siemens Building Technologies Identifies New Savings Opportunities
Energy audit review reveals additional system upgrades will cut energy use nearly in half
Buffalo Grove, Ill, Monday, September 29, 2008
Eastern Kentucky University will be reducing its carbon impact and its energy bill even more than it anticipated last spring when the school announced plans to team with Siemens Building Technologies, Inc., and embark on a comprehensive program designed to boost the energy efficiency of facilities campus wide.
After Siemens completed its energy audit of EKU facilities, a thorough review of its findings with the University’s facility management staff revealed that an additional $5 million in upgrades to energy-intensive systems would yield significantly higher savings—more than enough to cost-justify the now larger, $27 million investment. The performance-based sustainability project will be financed by a lease which will be paid back over a 13-year period from the energy savings guaranteed by Siemens once the system upgrades are completed.
Eastern Kentucky University President Dr. Doug Whitlock announced his decision to increase the scope of the project August 19 after reviewing the revised plan. “The Siemens sustainability project at Eastern Kentucky University is simply good business, from both an economic and environmental perspective. I’m pleased that the Siemens project has positioned EKU as a leader in energy efficiency in the Commonwealth and already brought positive national attention to Eastern. But most of all I’m excited that this innovative venture allows the University to achieve and advance its core mission while becoming an even better steward of the public trust and hard-earned taxpayer dollars.”
According to James Street, Eastern’s associate vice president of Capital Planning and Facilities Management, the guaranteed energy savings performance project focuses on upgrades and retrofits to energy-intensive building systems across the campus including heating, ventilation and air conditioning systems, lighting and other systems that consume water and fossil-fuel based energy resources like electricity and natural gas. “Eastern’s utility bill is approximately $6.4 million annually,” says Street. “With Siemens help we will be saving nearly $8,000 a day in energy expenses and when you add that up, we’re going to be cutting our on-campus utility consumption roughly in two.”
Siemens contract guarantees EKU will save 24,665,190 kWh of electricity, 89,329 mcf of natural gas, 1,729 tons of coal, 102,585 ccf of water and 138,584 ccf of sewer.The project’s impact on the environment will be as equally dramatic. According to Siemens over the 13-year period of the contract, Eastern’s energy savings will be comparable to removing 6,229 cars from the road, growing 227 acres of forest or not using some 79,000 barrels of oil. Similarly, over the contract’s duration Eastern will have reduced overall greenhouse gas emissions (CO2, NOx and SO2) by nearly 76 million pounds.