Skip to Content


Skip over secondary navigation

Secondary navigation

Content

For the business and trade press

Security, Delivered by Siemens, is Mission Critical for CityNAP Network Access Point and Communications Services Facility in San Antonio

Integrated video surveillance, intercom and access control assure facility’s security for client

BUFFALO GROVE, IL, Thursday, December 07, 2006

To assure its client’s sensitive data and vulnerable server hardware is safe and secure, CityNAP, a new internet hub and data center facility in San Antonio, has chosen Siemens Building Technologies, Inc., to deliver a comprehensive all-digital closed-circuit television security system to protect the new facility.

Designed to help nurture startup ventures and other high-tech enterprise, the 10,000-square-foot facility provides small, medium and large businesses with environmentally controlled and secure storage colocation with redundant power systems. CityNAP derives its name from the fact that it provides users with a dedicated network access point (a major junction on the Internet where two or more backbone networks are connected through routers to transfer data). Currently seven major fiber networks meet at CityNAP. It also provides access to several Internet service providers and has a fully wired conference room with a wide-screen plasma display which clients can use to make presentations and conduct video conferences.

Security is a mission-critical element of the company’s overall offering and CityNAP would not be in business if it didn’t take serious measures to assure that both data and equipment were protected from bad actors or other threats. “We knew from the very beginning,” says CityNAP president Frank R. Robles, “that physical security was every bit as important as information security to our customers. What’s called for on both sides of the security fence is a tightly integrated and comprehensive solution—and that’s why we chose Siemens.”

To thwart unauthorized access, facilitate transit and keep a watchful eye throughout the facility, Siemens implemented an end-to-end security solution that integrates digital video surveillance and intercom with an access control system across the facility’s high speed data network.

The access control system compliments Siemens HID Readers with Software House C•CURE® 800 technology and AIPHONE® IP intercom system. Digital video surveillance is accomplished via IPVision® enterprise software which manages the signal data from a strategically-placed array of IQinVision Mega Pixel cameras that provide high-definition quality video-enhancing security monitoring activities.  By integrating the intercom system into the IPVision console, security personnel can monitor cameras, respond to intercoms and perform door releases using the all-in-one application. In addition, CityNAP can use the IPVision console to manage all aspects of their facilities security from a single location or multiple locations.