Tools

Site ExplorerSite Explorer
Close site explorer

Tettnang Castle, Germany

Radio fire detection for Tettnang Castle with SWING

Customer

Tettnang Castle is beautifully situated in Germany’s Upper Swabia region. The high standards the Counts of Montfort-Tettnang held for their stately residence are still reflected in the castle today. Tettnang Castle was designed and furnished in the 18th century. Back then, only the best artists were engaged by the owner. The spectacular Baroque interiors are still among the finest in the region.

Tettnang Castle, Germany

Requirements

Filled with impressive art and stuccowork from the 18th century, Tettnang Castle is a historically important landmark. For the museum and the offices, which are housed in historical rooms, the customer needed a fire protection system that preserves the valuable interior in two ways: by reliable fire detection and by wireless installation.

Solution

SWING from Siemens proved to be an excellent choice to protect and preserve the historically valuable interior of Tettnang Castle. SWING uses mesh technology, which means that all wireless network devices communicate with their direct neighbors. This ensures outstanding connection reliability because at least two redundant paths are available to transmit information from the device to the gateway. SWING detectors were installed in the museum and the offices. They communicate with SWING gateways which are connected to a 4-loop control panel. In addition, wired detectors ensure reliable fire protection in the basement and attic of Tettnang Castle.

Benefit

The customer was very satisfied with the solution. Due to the intelligent and safe wireless technology SWING offers, the original building structure remained untouched. Moreover, SWING could be installed quickly without interfering with the museum’s opening hours.

Facts

  • 1 FC2040 control panel

  • 167 FDOOT271 SWING radio fire detectors

  • 10 FDCW241 SWING radio gateways

  • 133 FDOOT221 multi-sensor fire detectors

  • 13 FDM223 manual call points