Skip to Content
Skip over Language Selection
Skip over Primary Navigation
Skip over secondary navigation
Publishers Area
Skip over Contact, Sitemap
Skip over Search
[Advanced]
http://www.buildingtechnologies.siemens.com | Facts and Figures 2007 | 2008-03-12
print
Siemens Building Technologies continued its profitablegrowth in the past fiscal year. Profit once again showed a significant improvement.Building Technologies posted total revenue of 5.062 billion euros, an increase of 266 million euros (+6.0%) compared with the previous year. All divisions contributed to this growth. Due to the systematic selection of highly profitable projects, the increase in neworders was modest: 5.350 billion euros compared to 5.235 billion euros in the 2006 fiscal year (+2.0%).The positive trend in profitability has continued: Group profit of 354 million euros was 131 million euros or 58.7% higher than in the previous year. The profit margin therefore improved from 4.6% to 7.0%.
10/1/2005 -9/30/2006
10/1/2006 -9/30/2007
New ordersmillion euros
5,235
5,350
Salesmillion euros
4,796
5,062
Group profitmillion euros
234
354
Employeeson 9/30 (incl. trainees)
28,622
29,000