Skip to Content


Content

Protect your business, important assets, and the environment with Sinorix

When it comes to fire prevention, most businesses rely on sprinkler systems or, in some cases, a Halon system. Critical areas that contain your most vital assets and operations require a higher level of fire protection. The Sinorix system is an intelligent and customizable fire suppression solution that protects mission critical areas, prevents collateral damage, and enables business to continue as usual.

Sinorix Tank with Label from Siemens

Superior detection technology with fast suppression.

Our state-of-the-art fire suppression systems work with FirePrint™ Intelligent Fire Detectors, the most highly evolveddetection system available today. These detectors feature advanced micro-processing technology and function similarly to the human brain to discriminate between deceptive phenomena and an actual fire.

 
 

Sinorix 227

Detection, suppression and protection within seconds!

As a waterless fire extinguishing system, Sinorix 227 instantly squelches a fire before it becomes large enough to activate the sprinkler system. This protects critical assets and valuable items inside the building — from fire as well as damage caused by water. It’s an innovative and intelligent solution, with incorporatedfeatures that deliver peace-of-mind:

 
 

Sinorix 1230

Innovative, Intelligent and Environmentally Friendly

Sinorix 1230 is an innovative solution that reduces the risk of fire damage in critical applications, sensitive equipment areas, and at museums or archives holding rare and invaluable collections. The Sinorix1230 solution is based on a long-term, sustainable technology that has one of the highest safety margins in the industry and ensures quick and reliable extinguishing without a negative impact on the environment. It utilizes 3M™ Novec™ 1230 Fire Protection Fluid, an environmentally friendly extinguishing agent, that is safe at design concentrations, effective, and not subject to regulatory restrictions or phase out. Extinguishing via its cooling effect, Novec 1230 fluid works as a gas, yet it is a liquid at room temperature.

Environmental Performance guaranteed

The 3M™ Blue SkySM Warranty is a 20-year protection guarantee against regulatory bans or restrictions on the use of 3M™ Novec™ 1230 Fire Protection Fluid. If Novec 1230 fluid is banned or restricted for use as a fire protection agent due to ozone depletion potential or global warming potential, 3M will refund the purchase price of the fluid.

 
 

Choosing the Right Partner

A fire suppression system is only as good as the people who install and service it. At Siemens, we ensure quality by only allowing highly trained technicians from our Siemens branches and authorized partners to install Sinorix systems. This way you can be assured that your system will work when you need it most.

Siemens has been a world leader in protecting people, buildings, and assets for over 60 years. We are committed to providing safe, reliable, and sustainable solutions to our customers’ facilities. After decades of comprehensive analysis of fire-smoke data, extensive fieldwork, and testing in the world’s largest fire lab, we can confidently state that no one understands fire better than Siemens.

 
 

Sinorix™ Intelligent Fire Suppression

Catalog Sheets